NX Associative Measurement [Body] feature maintain relation to components

2021-10-06T23:27:39Z
NX for Design

Summary


Details

When a component in an assembly is replaced with a component that is not a version of the original component, an associative Measurement [Body] feature that includes the replaced component body and other components(s) is indicated as up to date. 

Shouldn't the user be made aware that the associative Measurement [Body] feature no longer include the original number of bodies selected?



Solution

Measurement [Body] feature is indicated as OK and associativity is still maintained to all the bodies (components) that were not replaced. 
User needs to edit the Body Measurement feature and add the replacement component. 
The Measurement command uses Selection Intent(SI), set to "Single Body", so the SI rule can be maintained when Measurement [Body] feature referenced geometry gets changed. Since with SI, user needs to do fully load part when the component replacement is done.



Notes and References

IR#7280347



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: DESIGN
Version: V1899
Function: INFO_ANALYSIS

Ref: 002-7006658

KB Article ID# PL7006658

Contents

SummaryDetails

Associated Components

Modeling